Part Number: TCAN4551-Q1
Tool/software:
Hi, TCAN4551-Q1 seems to be right on the project requirements, except that the CAN-driver is not isolated.
The data sheet describes a test mode where the built-in CAN-drivers are by-passed and the CAN-controller RX and TX are present at the GPIO-pins.
Is it possible/advisable to use this test mode to operate the CAN-controller together with an external isolated CAN-driver?
Best Regards,
Joakim Langlet