Part Number: DS90UB948-Q1
Tool/software:
Hi team,
Could you help me with two questions, thank you in advance.
Q1.
Current design is using "2-Lane FPD-Link III Input, Dual Link OpenLDI Output"

If we are change the design from current design to "1-Lane FPD-Link III Input, Dual Link OpenLDI Output",
Q1.1 will the image display normally?
Q1.2 What features will be impacted by this change?
Q1.3 Is the mapping of GPIOs on the SerDes pair affected?

Q2.
With spec of display screen(FHD 1920x1080) as below and use to "1-Lane FPD-Link III Input, Dual Link OpenLDI Output", Can frame rate reach 60fps?