Part Number: SERDESUR-43USB
Tool/software:
Hi
I want to use the SERDES De-serializer Board to show the Data of an Automotive Camera. The Cam has a DS90UR241QVS. I connected if to the De-serializer Board and the Board to a Display (TFT070-84NN). But i am a little bit confused, in the User Manual of the Serdes Demonstration Kit (Page 17), i can't get Information about the Output Data. In the Application Report SNLA102B–May 2008–Revised April 2013 (Page 2), i found informations about the Data. Is this true? To show a Picture i need RGB Data, Clk, HSync and VSync?
How can i change the Clock? In my case there are only round about 15MHz. The Display needs 33MHz. With the Serializer Board it should be possible to change the Clock using the Resistor at Port 23 "PRE" but at the Cam it is not connected.