Part Number: LMH0302
Other Parts Discussed in Thread: LMH0344, LMH0346
Tool/software:
Hi everyone. This is my first post, so please be patient if I make any mistakes.
My team designed two years ago a board to interface 3G-SDI inputs and outputs, with this part (LMH0302) used to drive the output. I am know testing the board with a Tektronix Waveform Monitor, and all I get is that signal is unlocked, even when the signal is a SD-SDI (576i).
After reviewing the design, I have discovered many issues about the layout, that could become a problem for 3G-SDI. But, is so critical the layout for SD-SDI? If not, what could be the problem so?
Inputs don't work either. We have used LMH0344 and LMH0346, and LMH0344 does not detect well when there is a signal.
I attach you the schematic. I don't think so, but maybe there is an issue there.
Thank you in advance.
Kind Regards.


Vmax ~= 400mV, Vmin ~= -400 mV -> Vpp ~= 800mV