Other Parts Discussed in Thread: DS64BR111, DS100BR210, DS100KR800, DS50PCI401
Tool/software:
The data sheet specifies that the device is a protocol-agnostic linear redriver that can operate for interfaces up to 25Gbps, including Ultra Path Interface (UPI) 2.0.
We are looking for a redriver that can be used on a 4Gbps 100 ohm Fibre Channel interface to connect two Fibre Channel ports between the Host ASIC and FR4 backplane/cable. Is this a suitable redriver part for our application? If not, can you recommend a part that would be suitable.