Part Number: TCAN1145-Q1
Tool/software:
Hello, the TCAN1145DMTRQ1 used in our product found that it could not communicate (the circuit diagram is below), and the chip was tested, please help analyze the cause of the problem;

Test 1: The waveform of CANH and CANL is measured as follows, the waveform changes to sawtooth wave, the waveform of CANH and CANL is the same, the amplitude is basically the same, and the period is 200us (5KHZ frequency);

Test 2: Comparing the waveforms of CANH and TXD/RXD simultaneously, it was found that the period of the sawtooth wave was consistent with that of TXD/RXD;




Test 3: The MCU cannot configure the mode of TCAN1145 through SPI.
Test 4: Change the TXD frequency to 500KHz through the MCU, and the test waveform result is the same as that of test 1;
Test 5: The resistance value of CANH to GND is about 11MΩ, the resistance of CANL to GND is about 11MΩ, and the resistance of CANH to CANL is about 125Ω(same as normal IC).
Test 6: After the MCU stops sending TXD packets, the CANH/L sawtooth wave disappears and becomes low.
Above, please help analyze whether it is the TCAN1145 chip damage? If the chip is damaged, please help confirm the cause of the damage? How to circumvent it?