Part Number: PLC010935BP
Other Parts Discussed in Thread: THS6222
Tool/software:
Hi,
I bought three boards for this experiment.
I put the two boards into transmitting and receiving mode respectively and directly connected their output terminals with wires.The results of the experiment are that all of them do not communicate except for 5MHz. For other frequencies that do not work, the carrier frequency remains in the D=1 section. Therefore, all are displayed as 0 during decoding, and communication does not occur.
In my opinion, I think that the filter works as a feedback line at lower frequencies. Therefore, I think that this circuit should have a function to stop the driver IC when receiving so that it works properly.
Is this a design flaw or am I misunderstanding something?
(Oscilloscope waveforms can also be sent upon request.)