Part Number: TCAN1145-Q1
Tool/software:
Hi Team,
We are using TCAN1145-Q1 to judge it is wake up frame from the network or not by CANINT register bit. While we found when there are other nodes receiving WUF, this TCAN1145 node cannot assert register bit when there is WUF on this node. (INT_ENABLE_1 register have been enabled).
During the test, as long as there are two nodes on the bus, one node sent out wake up frame, the TCAN1145 as another node can recognize the wake-up event. While when there are three nodes, one node sent out wake up frame, the TCAN1145 as another node cannot assert the register bit. Both conditions, the TCAN1145 can be wake up correctly, while we want to figure out why the wake-up event record result is different. Is there any restrictions for record the wake-up event by CANINT bit?
Sch:

Thanks
Best,
Frank