Part Number: UA9637A
Tool/software:
Hello, I'm trying to verify the following part number UA9637ACDR is interchangeable with DS9637ACM/NOPB but I can only find the datasheets for UA9637A and DS9637A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UA9637A
Tool/software:
Hello, I'm trying to verify the following part number UA9637ACDR is interchangeable with DS9637ACM/NOPB but I can only find the datasheets for UA9637A and DS9637A.
Hi Friedrich,
So the UA9637A is the device's general purpose name (GPN). The 'C' I believe stands for the temperature rating. The 'D' means the package type (SOIC). The R stands for reel (like in a tape and reel). So the datasheet for UA9637ACDR would be the same datasheet UA9637A (we go by the GPN for datasheets).
DS9637A is the GPN. 'C' refers to the operating temperature range (0C to 70C). And I think the M stands for military (I want to say this means it goes through more thorough final tests or other qualifications but I'm not too familiar). I believe NOPB denotes the SOIC package but for military products. Use the datasheet for the DS9637A GPN, the commercial and the military part share the same datasheet.
In short, both datasheets you are seeing are correct for the GPN.
| UA9637A | DS9637A | |
| Number of channels/receivers | 2 | 2 |
| Vcc support | 5V | 5V |
| Pinout same as other compared device | Yes | Yes |
| Vth+ | 0.2V | 0.2V |
| Vth- | -0.2V | -0.2V |
| Typical Hysteresis | 70mV | 70mV |
| Max prop delay low to high | 25ns | 25ns |
| Max prop delay high to low | 25ns | 25ns |
| Max support common mode | +/-15V | +/-15V |
| Max Short circuit current | 100mA | 100mA |
Overall, I see the two device's electrical parameters as exactly the same. I suspect the DS device was a copied spec from the UA9637 device. My guess is National Semiconductor (TI acquired them around 2010) was trying to make a pin to pin version of the UA9637A device which is why the specs look the same.
-Bobby