Tool/software:
I have a question regarding the values of pull-up and pull-down resistors for bootstraps in the TI_DP83826E.
The datasheet recommends a pull-up resistor value of 2.49kΩ and a pull-down resistor value of 1.5kΩ.
It is also stated that the recommended tolerance is 1%.
On the other hand, the bootstrap has two levels, with VH minimum at 1.3V and VL maximum at 0.6V.
The internal pull-up and pull-down resistor values are both 10kΩ ±25%.
Considering the threshold values and internal resistor values, is it acceptable to use pull-up and pull-down resistor values other than 2.49kΩ and 1.5kΩ for bootstraps?
Why is a 1% tolerance recommended?