Part Number: TCA9539-Q1
Tool/software:
How much current of TCA9539-Q1 VCC? How to understand 160mA? In 6.5 and 6.9 chapter, ICC is not over 1mA, is in uA level, my question is, when calculate power current, which current is right?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9539-Q1
Tool/software:
How much current of TCA9539-Q1 VCC? How to understand 160mA? In 6.5 and 6.9 chapter, ICC is not over 1mA, is in uA level, my question is, when calculate power current, which current is right?

So, how many current is required when we calculate this IC power consumption?
from chapter 6.5 and 6.9, under 1mA?
Hi Xin,
Clemens is correct here.
For example, if you had P00 set to an output HIGH with a 1k load to GND at VCC = 3.3V, then you effectively have a load current roughly equal to 3.3V / 1000 ohm = 3.3mA flowing from VCC out of the P00 pin, to GND.
For total worst case load current, you would need to conduct a similar analysis for each pin. Each pin load varies dependent on the type of pin configuration INPUT/OUTPUT, and the load that is being driven. Consider that some pins will be high-z inputs, some pins will drive output HIGH, output low, some drive LED's etc.
Each pin will have some type of current load. The sum of all of these loads is the worst case current.
IF you are trying to see the break point of the device, check the abs. max conditions in the datasheet. I believe the total current that can flow out from VCC or into GND is in the 100's of mA.
Regards,
Tyler