Part Number: USB-TO-GPIO2
Other Parts Discussed in Thread: BQ78PL116
Tool/software:
We have a a problem with some of the last USB-TO-GPIO adapters we received.
Some work and some cannot be connected -> "unable to connect to device, please check power and the connections to the hardware."
Also a Firmware change or update is not possible -> "no adapter found!"
The Version of the USB-TO-GPIO is the first one without a "2" in the end.
USB-TO-GPIO
LOT: 362520KRY
TKY(1T) 6202135ZE9
LBL: 17A (L)TO:1185
Is there anything we can do to make them work?
Since they seem to be discontinued and replaced by the Version USB-TO-GPIO2 we cannot buy them anymore.