Part Number: DP83822I
Tool/software:
Greetings! I am using this part for a very first time! I have connected DP83822 to Xilinx Zynq. The problem is the communication between the Zynq and DP83822 is not OK. For example I can set registers through the DPIO, but when I try speed autonegotiation for example, I can set the corresponding flags, but the flag auto-negotioation completed never goes high. I on the Zynq side I always receive a message Phy setup error and Ethernet Link down. It is the same when I use preset speed. Can you check my schematic? Have I`ve done something wrong? The Zynq side is working on 1.8V and I have supplied the VDDIO with 1.8V in order to make the IO pins of the DP83822 workinDP83822 TI.pdfg on 1.8V..
Do you see anything wrong?
Thanks!