Part Number: TCAN1051HG-Q1
Other Parts Discussed in Thread: ISO1044, ISO1050, ISO1042-Q1
Tool/software:
Hello Team,
We have a system with can interface and the transceiver using is TCAN1051HGVDR.
The CAN signals are taken through twisted pair cables only but they had to travel through a breakout box, wiring harness before reaching the 2nd CAN device.
We have termination resistors of 120 ohms on both CAN sides.
The resistance between the CAN H lines between either end is almost 5 ohms similarly for CANL lines (Measured with a multi meter, the breakout box, and harness add the line resistance.)
1). Will this resistance create any problem?.
2). Do we need a GND lines along with CANL and CANH lines between the CAN devices as they are working with 2 different power supplies and the GND is not connected together?.
3). We have a junction box connected at the breakout box side and 2 CAN analyzer devices are connected at the junction box.
Since each are CAN nodes, which is the ideal place yo connect the termination resistor?.
4). Sometimes we have to add an extra 120 Ohms resistance at the analyzer side for proper communication (the effective resistance will be 40 Ohms). Why is this?.

Looking for your reply