Part Number: TCAL6408
Other Parts Discussed in Thread: DAC63004,
Tool/software:
Hi TI,
It is not a question but a suggestion. Why do not you allow for four I2C addresses instead of just two?
Additional two addresses could be easily handled the same way DAC63004 does it, that is, by connecting ADDR pin to either SCL or SDA.
This would be a great improvement while pin and functional compatibility would be 100% retained. It seems like it is a really 'low hanging fruit'.
Ofc, I know that similar IC with more ports exist but it is not a desirable solution since it would require more long PCB tracks (SCL/SDA is routed anyway) which even may force us to add additional PCB layers.
In such context, using, let's say, four 8 port expanders, rather than two 16 port expanders would be substantially more convenient and actually dramatically cheaper.
Kind regards,
Thomas