Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Tool/software:
Hi, I'm using DP83869 as a media-converter. Now I need to send some data just at linkup. I think PRBS function can give what I need. But I can not received any packet on the other side.
The topology I used is as follows:
PC1-->media-converter with DP86869-->fiber-->TP Link media converter-->PC2
Packets between PC1 and PC2 can be sent and received correctly in normal operation. Now I need send a few data from DP83869 to PC2 just at beginning with PRBS.
I just write reg 0x16 with 0xF000, where loopback not needed. But I can not receive any packet at PC2. So two questions:
(1) Do I need to config other registers besides reg 0x16 if I do not use loop back and just send out some data?
(2) Does PRBS works if DP83869 in media-converter mode? And if it works, is the PRBS enable register address still 0x16?
Thanks.