Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Delays in IC packages

Part Number: DP83867IR

Tool/software:

Hi Team,

The customer uses DP83867IRRGZT with RGMII 1000Mbps.

They aim to adjust the timing using only the delays caused by the pattern on the PCB, without using clock shift modes.

How much internal delay do the TX line(TX_D[3:0], TX_CLK, TX_CTRL) and RX line(RX_D[3:0], RX_CLK, RX_CTRL) signal lines have within the IC package?

They are trying to design the pattern length taking into account the internal delay of the IC package.

Best Regards,