Part Number: TCA9406
Other Parts Discussed in Thread: TXS0102, ,
Tool/software:
Hello,
I have seen similar questions on the forum but I'm not sure I understand if this is possible or not.
In our application, we have: VCCA = 2.5V and VCCB = 3.3V.
On power-up, VCCA goes up first and VCCB remains low down by default.
When necessary, the embedded processor enables VCCB (in order to communicate with the component on the B-side of the level-shifter).
From what I understand from the datasheet, OE must be tied to ground through a resistor until VCCB is powered-on, and only then OE can be set high to enable the device.
Since VCCA is the first voltage rail to be powered-on, OE cannot be tied directly to this rail.
Is it possible to tie OE to VCCB then?
We could also use the embedded processor to drive OE, but we want to minimize the I/O pin count in our system.
In the same design, we are also wondering if we can do the same thing for a TXS0108 (tell me if I'm wrong, but I understand that the TCA9406 is identical to the TXS0102).
Thank you for your help.
Maxime