Part Number: PCA9555
Other Parts Discussed in Thread: TCA9535
Tool/software:
Hi team,
If config one of I/O port as input which has pull-up resistor, like below picture shows. Will the pull-up resistor impact the output of I/O and can't recognize the logic correctly?
For example: When P01 is initialized, P00 as an input port will read a high level due to the presence of a pull-up resistor. When the activation level of the input signal is also high, how to distinguish whether it is a high level caused by the pull-up resistor or a high level of the external input?
How to implement Open-load and other diagnostics for the P01 port?

Best,
Josh