Part Number: TCAN4550
Tool/software:
Hello, TI Team.
I am using TCAN4550 for my system with STM32H series MCU.
and in the datasheet of TCAN4550, there is max sck rise/fall time of 10ns. (trsck, tfsck)

But in my system, when I checked with sck rise/fall time with oscilloscope, as below tr/tf are about 8~9ns.Almost to Spec.
Will it be any problem?
There is no damping R or cap in the spi sck line between MCU and TCAN4550. SPI Lines are directly connected.
Main clk 40Mhz is very clean.
Our FW Engineer says that there are some missing datas and some garbage data comes out from CAN Line.
So I'm looking into whether it might be related to the HW issue.
Thanks.