Part Number: TCAN1043G-Q1
Other Parts Discussed in Thread: TCAN1043
Tool/software:
Hi TI member,
We have a CAN test problem need your help.
As below is our schematic connection of CAN tranceiver.
We encountered an issue with the CAN transceiver — an abnormal output on the nFAULT pin.
As shown in Figure 1, our CAN architecture has one shared output (U299 & U300). When testing packet transmission between the two CANs, U299 continuously outputs nFAULT (see Figure 3), though there is no packet drop or error in CAN transmission, and the other side (U300) does not output nFAULT. We can't confirm what kind of anomaly this is (refer to the datasheet, maybe TXDDTO/TXDRXD).
We conducted the following tests for this issue:
1. Swapping U299 with the standalone U523 on the right side, neither CAN exhibited abnormal output on the nFAULT pin.
2. Moving U299 to U300's position. then U299 will keep the nFAULT pin abnormal output.
Based on these tests, we believe the issue may be related to the electrical characteristics of the CAN transceiver, as there seems to be a compatibility issue. U299 exhibits this issue in the shared circuit but does not when moved to another position, whereas U300 and U523 show no issues in either position.
This issue has appeared in 5 out of 1,500 DUTs. We would appreciate your assistance in confirming if similar issues have occurred before or if you have any recommended directions for analysis.
Thank you.
Fig1: U299 & U300 connection

Fig2: V31C/V31U CAN Failure

Fig3: nFAULT continue output