Other Parts Discussed in Thread: SN65LVCP418, SN65LVCP408
The outputs of the SN65LVCP418 can be put into a 3-state mode. It appears that a register must be set through I2C. In Table 4 of the datasheet, bit 2 of the output port control registers whose function is to 3-state the port shows up as a read only bit. I feel like it should be R/W. Is this an error in the documentation or is there something I'm misunderstanding?