Part Number: DP83867IS
Tool/software:
Hi All,
Could you please tell me about the DP83867IS?
Customer reboot my STB periodically, but sometimes after rebooting I can't communicate over Ethernet.
The configuration is as follows:
IoT router → DP83867IS → STB (Set top box)
From the IoT router, the DP83867IS's LAN LED is on and it appears to be linked via 1000BASE.
However, communication is not possible. (There is no ping response from the other side)
The other side's STB also appears to be able to maintain the link based on the status of the LAN LED.
> [45092.751482] pfe 4000000.pfe eth0: Link is Down
> [45093.791595] pfe 4000000.pfe eth0: Link is Up - 1Gbps/Full - flow control off
> [45097.963678] pfe 4000000.pfe eth0: Link is Down
> [45098.991351] pfe 4000000.pfe eth0: Link is Up - 1Gbps/Full - flow control off
> [45202.385176] pfe 4000000.pfe eth0: Link is Down
> [45206.111797] pfe 4000000.pfe eth0: Link is Up - 1Gbps/Full - flow control off
However, the LINK LED does not appear to be off when LINKDOWN occurs.
Is there anything else I should check?
Please tell me how to isolate the cause.
Best Regards,
Ishiwata