Part Number: TCA9517-Q1
Tool/software:
Hi,
I have couple of basic questions.
1. Can I leave the EN pin floating? Will the device be fully functional if this pin is floating
2. The datasheet mentions about problems in connecting the B-Side to another B-side device. I did not fully understand the problem - I believe the issue is that the VOL of B side output is 0.5V and since the VIL of B side needs to be 0.43V or less, we cannot connect B side to B side. Am I correct in my understanding? In my application, we dont have multiple I2C buffers. In that case, can I connect B side to any target device as long as the Vol of that target device is less than 0.43V? I am planning to connect the B-Side to the Power supervisor IC "UCD9090ARGZR". Will it work?
Regards,
Veerasamy