Part Number: TCAN1145-Q1
Tool/software:
Hi team,
The CAN transceiver used in the customer project is TCAN1145. Recently, two after-sales parts in the actual car cannot be awakened;
The wake-up solution is to wake up with a specific message and wake up the MCU through the INH pin;
1. During the bench test, it was found that constantly short-circuiting CANH and CANL to artificially cause BUSOFF, which occasionally causes the CAN transceiver to be unable to wake up after sleeping;
2. At this time, the INH pin is always low, and sending a wake-up message cannot wake up, and the INH pin has no action;
3. Short the INH pin to the power supply and artificially trigger the wake-up pin. The MCU can wake up normally, proving that the MCU wake-up logic is fine;
4. After forced wake-up, the INH pin still maintains a low level, but CAN communication can be normal at this time;
5. The power must be turned off to recover;
Please help analyze under what circumstances will cause the INH pin to be low and unable to wake up;