Part Number: DS80PCI402
Tool/software:
Hi, Dear supporter,
I am using DS80PCI402 to boost a 2x PCIe connection. If I using pin mode, set pin state as following, the EP device can be enumberated by host.
|
ENSMB |
1K to GND |
|
EQA[1:0] |
1K to GND, 1K to GND |
|
EQB[1:0] |
1K to GND, 1K to VIN |
|
DEMA[1:0] |
Float, Float |
|
DEMB[1:0] |
Float, Float |
|
LPBK |
Float |
|
VDD_SEL |
GND |
|
SD_TH |
Float |
|
/PRSNT |
LOW |
|
VIN |
3.3V |
Then I tied ENSMB to VIN to access the device from SMBUS, according to the table above, I set,
EQA0/1 = 0x00
EQB0/1 = 0x03
DEMA0/1 = 0x02
DEMB0/1 = 0x02
VOD = 0x05
However, the EP cannot be enumberated by host. Therefore,
1) Is there a way to read registers out by SMBUS when chip is in PIN mode? If yes, I can read the configuration out in PIN mode as a starting point for SMBUS mode.
2) I've provide the register dump and schematic as below, could you please help to analyze?
Data read from device:
0000: 40 00 00 00 00 00 10 01 00 00 cc 70 00 00 08 03
0010: ad a2 00 00 00 08 03 ad 82 00 00 00 00 2f ad 02
0020: 00 00 00 00 2f ad 02 00 0c 00 00 08 00 ad e2 00
0030: 00 00 08 00 ad e2 00 00 00 00 2f ad 02 00 00 00
0040: 00 2f ad 02 00 00 38 00 05 00 00 00 00 00 00 00
0050: 00 44 00 00 00 00 10 44 21 00 54 54 00 00 00 00