Part Number: TVS2701
Tool/software:


- Vin MAX (gateway) = 28,8Vdc
- Vin DC/DC MAX = 34V (above this value the DC/DC can be damaged).
- External choke:
- Positive winding open.
- Negative winding seem ok.
- TVS2701DRBR is not in short circuit, but I can't test if it's ok or if it's broken (open).
- C193 is obtained by 2 multilayer ceramic capacitors (1210 10uF50V X5R) mounted in parallel (physically one on the other). One of these is shorted after surge tests (I can see a fracture in the ceramic body).
- Is TVS2701DRBR the correct choice in this context?
- Can I say that the problem would be caused all by the external common mode filter or I must to expect to have the same problem with the filter inside after the TVS?
- Is the design scheme correct or do you see some critical points?
- If necessary an hw modification the ideal is to be able to make it on the fly and in a second time to modify the PCB, so to end the whole tests.