Part Number: TS3USB221
Tool/software:
Hi alll,
I have a question about PCN:20241101001.0. for TSUSB221RSER
When the revision was changed from Revision J (January 2019) to Revision K (July 2024), the following changes were made.
• Changed the typical bandwidth value from: 1.1GHz to: 1GHz........................................................................... 1
I checked both the SCDS220K and SCDS220L datasheets, but could not confirm the above changes.
Is it correct to assume that this applies only to the TS3USB221RSER, i.e., the UQFN package?
Also, if it is limited to the UQFN package, when will this be specified in the datasheet?
The following items remain at 1.1GHz.
Page 1:

PAGE 6:

Thanks in advance.
Regards,
Toshi