Part Number: TCAN1145-Q1
Tool/software:
In the DS section 10.6.33 on sheet 83, the SW_RSVD_y register is defined to be three addresses, 41h, 42h, 43h, so three Bytes
The DS table 10-19 on sheet 68 "Register Name" says "SW_RSVD0 through SW_RSVD4", so five Bytes, which would require additional addresses.
Should table 10-19 say SW_RSVD0 through SW_RSVD2"
Also note that the 10.6.33 says: "Register address 41h through 43F" so should be "...43h"
Thanks,
Mark