Part Number: DS320PR1601
Tool/software:
Hi,
We have used Broadcom's eye diagram drawing software to draw the eye diagram of DS320PR1601 REDRIVER.
We have tried all the EQ combinations so far, and only a few can link gen5, but the performance is not good. If the eyes are not opened, the mask will hit.
The first attachment is the eye diagram of the redriver, and the second attachment is the eye diagram of using the 2meter QDD CABLE loop back without the redriver.
There should be no problem with the signal. I don’t know if the gain of the driver is not large enough. we refer to Broadcom’s spec here what is sent is 36DB. The maximum GAIN of DS320PR1601 seems to be only more than 20DB.


Jeff