Part Number: THVD4431
Tool/software:
Hello,
I am currently building a seriel interface with the THVD4431 multiprotocol transceiver in connection with an PCIe UART IC (XR17V354, MaxLinear (former Exar)).
The UART IC contains a so called 'auto RS485 half-duplex direction control' feature which i would like to integrate in my design.
It is stated that the UART IC uses either the RTS or DTR Pin to activate it. (In my case L4 or L6)
In my understanding, in RS-485 half or full-duplex mode these pins are not relevant.
I saw in old designs that the RTS/DTR Pin is bridged with the DIR Pin of the transceiver.
My Questions are now:
1. Does the connection of RTS/DTR to DIR also apply to the THVD4431 to realize the auto RS-485 feature?
and if so
2. Does this connection affect the RS-232 3T5R mode? (I couldn't find proper information about the DIR Pin state in RS-232 3T5R mode in the data sheet)
Or am I on the complete wrong path?
Thank you in advance for answering.
Regards,
Jan