Part Number: ESD204
Other Parts Discussed in Thread: TPD4E02B04
Tool/software:
Hello,
I currently use an OnSemi ESD8004 which appears similar to the ESD204DQAR. The OnSemi part is not only obsolete, but I've also had issues with it getting damaged somehow in the below circuit.
The circuit detects when a certain battery type is plugged in, there is a pull down resistor in the battery and then the pull up on this circuit, therefore creating a divider that triggers a comparator based on the measured voltage. I've had this ESD8004 device get damaged, with either a short to ground or some current draw to ground which causes a "detection" on my circuit when nothing is attached. I am unsure how this is occurring, but I'd like to change to the ESD204DQAR from TI, do you see any issues with this circuit using the ESD204? The expectation is that no current should conduct through the ESD device when there is no ESD event, or if there is a current its miniscule and wouldn't be enough to create a sizeable voltage drop across the 10k pull up resistor.
Only 1 channel is shown in that 4 channel part, the other 3 have SDA/SCL on 2 of the lines, and another identical circuit for a different type of battery on the 3rd channel.

Thanks,
Mike