This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF230: Power Sequence Related

Part Number: DS250DF230

Tool/software:

Hi TI team,

READ_EN_N, INT_N, SCL& SDA are 3.3V tolerant.

Just wonder any concern if we supply 3.3V first before 2.5V VDD?

Thanks.

  • Hi Alfred,

    This falls within the absolute maximum ratings of the device.  We would not expect damage from this condition.

    Please also note that exposure to absolute-maximum-rated conditions for extended periods may affect device reliability.  Because of this, I would not recommend designing a system where 3.3V is supplied for an extended period without 2.5V.  I think this would not be the case in your system where 3.3V is supplied for a short period of time prior to 2.5V.

    Thanks,

    Drew