Part Number: DS90UB962-Q1
Tool/software:
Hello TI,
We are using ti962 to connect 4 camera(ser is ti933) . We would like to find out register for spread but nothing find except for this:
As an option for mitigating EMI / EMC, the DS90UB962-Q1 is capable of tolerating a REFCLK with spreadspectrum clocking (SSC) profile with up
to ±0.5% amplitude deviations (center spread) or up to 1% amplitude deviations (down spread) and up to 33-kHz frequency modulation from a clock source
Is ti962/933 support spread setting by device register? Thanks.
Thanks.
Wufeng