This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Mimimum external pull-up resistor value for RX_ER strap pin

Part Number: DP83822I

Tool/software:

Hello,

I have a question for a strap configuration.
In my customer case, the RX_ER of DP83822 is connected to AM335x's MII1_RX_ER pin which has an internal pull-down (51~210uA, 3.3V)
They want to set the RX_ER strap to Mode 4. Then they are considering to put an extenral pull-up on the line.
To set it to Mode 4, it may requires 3~4Kohm level pull-up at least. Is it OK to add this leve of pull-up on this line for proper operation?
Or do they need to add a switch to cut the pull-up after the strap timing?

Regards,
Oba