Part Number: ESD321
Other Parts Discussed in Thread: ESD122, , STRIKE
Tool/software:
Hi All,
I have some questions about ESD321 and ESD122.
(1) The ESD321 has one diode circuit. The ESD122 has two diode circuits.
What are the advantages and disadvantages of having one diode circuit and having two diode circuits?
(2) Is the ESD321 effective against negative ESD? If so, please explain how it works.
(3) Is there a graph for the ESD321 that is the same as Figure 4. –8-kV IEC 61000-4-2 Waveform, IO Pin to GND in the ESD122 datasheet?
In the ESD321 datasheet, it says Figure 6-4. 8-kV IEC 61000-4-2 Clamping Voltage Waveform, GND to I/O Pin.

Best Regards,
Ishiwata