This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: Value of Capacitor Connected to the Center Tap of RJ45 Pulse Transformer

Part Number: DP83826E


Tool/software:

Hi team

Is there a specified or recommended value for the capacitor connected to the center tap of the RJ45 pulse transformer?

The datasheet indicates 2nF, while the evaluation board (EVB) uses two 0.1μF capacitors.

Do you have any guidelines for the settings?

Thanks