Part Number: DP83TC811-Q1
Other Parts Discussed in Thread: DP83TC811
Tool/software:
Hi Team,
i am having issues with the RX of the DP83TC811. ethtool shows it is due to CRC errors. The testsetup is:
mac <-> dp83tc811 <-> rddrone t1 adapter <-> router
I configured the dp83tc811 to be in RGMII mode. I did check the SQI register and it indicates good link status. What can i do to further debug the issue ?
# ifconfig eth0
eth0 Link encap:Ethernet HWaddr 96:B0:87:97:E4:BC
inet addr:192.168.179.154 Bcast:0.0.0.0 Mask:255.255.255.255
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:1433 errors:1470 dropped:1 overruns:0 frame:1470
TX packets:333 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:101042 (98.6 KiB) TX bytes:18314 (17.8 KiB)
# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: Not reported
Supported pause frame use: Symmetric
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: Not reported
Advertised pause frame use: Symmetric
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Port: Twisted Pair
PHYAD: 1
Transceiver: internal
Auto-negotiation: off
MDI-X: Unknown
Supports Wake-on: g
Wake-on: d
Link detected: yes
#ethtool -S eth0
...
rx_packets: 2996
rx_broadcast: 1430
rx_multicast: 92
rx_crc_errors: 1474
...