Part Number: TCAN1043A-Q1
Tool/software:
Hello team,
TCAN1043A can be used in 24V system, but the Vsup pin cannot connected to KL30, because the input range is only up to 40V.
So generally, a primary voltage converter is needed, which causes another problem: system cannot meet low quiescent current requirement, usually no more than 100uA.
My idea is adding a dedicated WV Buck powered for Vsup only, and set 1043A in standby mode, the buck will be enabled by INH signal.
However, there are two drawbacks: 1. buck will bring more cost, 2. the buck causes more quiescent power loss.
So, do you have any better solutions? Thanks!
Regards,
Daniel Wang