Part Number: TCAN1043A-Q1
Other Parts Discussed in Thread: TCAN1043
Tool/software:
Hello team,
1. from the data sheet I have observed , when using a remote wakeup capability specific pattern of CAN frames needs to be put in CAN bus to make INH high - is this assumption is true or TCAN1043 will make INH high for any bus activity

2.Referring to the above block diagram,lets assume initially INH is low and system is completely turned off since no 5V output , If I want to put my system back to normal mode , I have to INH high to turn on the buck converter, i order to do so by remote wakeup , if CAN bus experience any signal will my INH will go high ? if not what is the constraint have to be followed w.r.t CAN frames.
3.assume now the system is in normal mode, I have to make INH low to cut down the power to the entire system so that system is in completly sleep mode , so what is procedure or sequence has to be followed w.r.t Stb pin and EN pin in order make INH low .
4. system has either completely turned off - sleep mode or should be normal mode - this is our expect ion that has to achieved through CAN INH signal.
Please provide the solution for the above queries