Part Number: DP83826I
Tool/software:
Hello,
We are using the PHY device DP83826I (in Basic mode) with the processor through MII interface in our hardware board design. The block diagram and schematic is attached for your reference.
Schematic_DP83826I_27NOV2024.pdf
We have configured the PHY device, DP83826I in the MII MAC mode using the strap pins. So, we have probed RX_CLK, TX_CLK pins using oscilloscope and observed a perfect 25MHZ clock signal on these pins.
The register dump from 00h to 3fh and register values of 467h, 468h is attached below for your kind reference.
The strap pins in the schematic is same as per the data stored in the register 0x467h (mentioned in the register dump).
"Broadcom XGS IProc Ethernet driver 0.1 bcm_xgs_eth_init enter Initializing GMAC1 gmac_mac_init: Chip ID: 0xb260 Connect bcm_xgs_gmac-1 to Generic PHY bcm_xgs_gmac-1 ethernet functionality initialized eth0: bcm_xgs_gmac-0, eth1: bcm_xgs_gmac-1 [PRIME] u-boot> mdio list bcm_xgs_gmac-0: bcm_xgs_gmac-1: 1 - Generic PHY <--> bcm_xgs_gmac-1 u-boot> mii info PHY 0x01: OUI = 0x80028, Model = 0x11, Rev = 0x01, 100baseT, FDX PHY 0x18: OUI = 0x180361, Model = 0x19, Rev = 0x05, 10baseT, HDX u-boot> mii read 0x1 0-3f addr=01 reg=00 data=3100 addr=01 reg=01 data=786D addr=01 reg=02 data=2000 addr=01 reg=03 data=A111 addr=01 reg=04 data=01E1 addr=01 reg=05 data=CDE1 addr=01 reg=06 data=000F addr=01 reg=07 data=2001 addr=01 reg=08 data=0000 addr=01 reg=09 data=0000 addr=01 reg=0a data=0102 addr=01 reg=0b data=0009 addr=01 reg=0c data=0000 addr=01 reg=0d data=0000 addr=01 reg=0e data=0000 addr=01 reg=0f data=0000 addr=01 reg=10 data=0015 addr=01 reg=11 data=010B addr=01 reg=12 data=6400 addr=01 reg=13 data=2800 addr=01 reg=14 data=0000 addr=01 reg=15 data=0000 addr=01 reg=16 data=0100 addr=01 reg=17 data=0049 addr=01 reg=18 data=0400 addr=01 reg=19 data=8C01 addr=01 reg=1a data=0000 addr=01 reg=1b data=007D addr=01 reg=1c data=05EE addr=01 reg=1d data=0000 addr=01 reg=1e data=0102 addr=01 reg=1f data=0000 addr=01 reg=20 data=3100 addr=01 reg=21 data=786D addr=01 reg=22 data=2000 addr=01 reg=23 data=A111 addr=01 reg=24 data=01E1 addr=01 reg=25 data=CDE1 addr=01 reg=26 data=000D addr=01 reg=27 data=2001 addr=01 reg=28 data=0000 addr=01 reg=29 data=0000 addr=01 reg=2a data=0102 addr=01 reg=2b data=0009 addr=01 reg=2c data=0000 addr=01 reg=2d data=0000 addr=01 reg=2e data=0000 addr=01 reg=2f data=0000 addr=01 reg=30 data=0615 addr=01 reg=31 data=010B addr=01 reg=32 data=0000 addr=01 reg=33 data=0000 addr=01 reg=34 data=0000 addr=01 reg=35 data=0000 addr=01 reg=36 data=0100 addr=01 reg=37 data=0041 addr=01 reg=38 data=0400 addr=01 reg=39 data=8C01 addr=01 reg=3a data=0000 addr=01 reg=3b data=007D addr=01 reg=3c data=05EE addr=01 reg=3d data=0000 addr=01 reg=3e data=0102 addr=01 reg=3f data=0000" "u-boot> mii write 0x1 0xd 0x1f u-boot> mii write 0x1 0xe 0x467 u-boot> mii write 0x1 0xd 0x401f u-boot> mii read 0x1 0xe 0086 u-boot> mii write 0x1 0xd 0x1f u-boot> mii write 0x1 0xe 0x468 u-boot> mii write 0x1 0xd 0x401f u-boot> mii read 0x1 0xe 0187"
# PRBS Check using BIST Control Register (0x16h)
We have also done PRBS testing using BIST Control register (0x16h) by connecting a RJ45 cable to the RJ45 connector of the PHY and shorted TX and RX of the RJ45 cable and checked the register 0x16h and as per our understanding, it is working fine. Register dump of the same is also attached.
u-boot> mii info PHY 0x01: OUI = 0x80028, Model = 0x11, Rev = 0x01, 100baseT, FDX PHY 0x18: OUI = 0x180361, Model = 0x19, Rev = 0x05, 10baseT, HDX u-boot> mii read 0x1 0x16 1 0100 u-boot> mii write 0x1 0x16 0x3100 u-boot> mii read 0x1 0x16 1 3B00 u-boot> mii read 0x1 0x16 1 3B00
The main problem arises whenever we connect our Hardware board with the external PCB, the link established but ping always fail.
Please let us know the reason for this ping failure.
Regards,
Santosh