Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB924-Q1: Cable length

Part Number: DS90UB924-Q1

Tool/software:

Hello team,

Can you help clarify the cable length value for the circle marked, range is also ok.

Thanks!

Regards,

Daniel Wang

  • Hi Daniel,

    Long cable mode really depends on the channel quality. Basically, Long Cable mode will simply start the AEQ floor value at a higher start point. If the minimum AEQ floor value is much lower than the typically settled value, then you can select the Long Cable mode.

    In general, you can enable long cable mode if the cable is over 5m long, but again, for the length of the cable, the full end-to-end system (device, traces, connector, and cable) should meet the channel specifications, including IL and RL to maintain signal integrity.

    Best,

    Josh