Part Number: SN65HVD230
Other Parts Discussed in Thread: TCAN1057A-Q1
Tool/software:
Hi,
I am evaluating to change the CAN driver for the SN65HVD1050DR.
Both part numbers are pin to pin compatible but the voltage range is different.
For the SN65HVD230, the recommended voltage range is 3 to 3.6V and the maximum rating 6V.
For the SN65HVD1050DR, the recommended voltage range is 4.5 to 5.5V and the maximum rating 7V.
What are your opinion about problems that this could have?
BR
Luis