Part Number: SN65C1168
Tool/software:
Hi
How many watt is required for the power supply Vcc input to make sure the IC can work correctly ?
in our application we are transmited 2Mbps over 100 meter cable.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The worst-case idle current is 9 mA for the driver and 9 mA for the receiver. The typical load current for 100 Ω termination is 2× 31 mA; the maximum is somewhat higher, but not specified. The additional supply current for switching at 2 Mbps it not specified, but you can assume something less than about 2× 20 mA. If you want the circuit to be able to handle a shorted outputs without the supply dropping out, then it must be able to handle more than 2× 150 mA.