Part Number: LMH0397
Tool/software:
Hello,
We have a PCB with the LMH0397 chip. We want to test what the maximum length of the cable is to still receive the SDI signal.
On the first PCB, we use SDI IO as input and SDI out0 as output. We then connect our cable to the out0 and connect it to the other PCB on in0.
We then test the signal we get from the second PCB on SDI OUT.
Furthermore, we did a couple of tests, and if the cable is under 10 meters long, we get a signal on the output without any issues.
On longer cables, we start having issues. We get either no lock at all or the lock LED starts blinking instead of being constantly on, like with our successful tests.
We do have access to the SPI communication with the chip, and we tried changing a few settings. We changed out0 VOD and de-emphasis registers, which improved the signal a little bit.
We would like to know what would be the optimal register configuration for our setup that would allow us to get a signal on the output with the longest possible cable.