Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Tool/software:
HI,
I would like confirmation of my understanding about a point on the DP83869 in 1000Mbps Media Converter Mode.
I would like to use the DP83869 with unmanagement and therefor ;
1 - I would like to know if the strap hardware configuration:


2 - And the configuration register :
• Write 0x0044 to register 1DFh // Set Operation Mode to 1000Base-T to 1000Base-X
• Write 0x1140 to register 0h // Reset BMCR
• Write 0x5048 to register 10h // Reset PHY_CONTROL
• Write 0x1140 to register C00h // Reset FX_CTRL • Write 0x4000 to register 1Fh // Software Reset
Question_2 : it is mentionned that 0x1FFC should be write to register 0x1EC in the SNLA318-February 2019 => Do I write this ? Where I should write it : first or there is no matter ?
are sufficient to insure operational link ?
Thank you
Regards
Fabrice