Tool/software:
Hi.
I am currently using this product (THVD1450DRBR) and I have a question regarding the termination resistor for RS-485 A and B.
The temperature of the termination resistor increases when the power to the controller is turned on.
I'm only using the driver side and have set the pull-up for DE and nRE.
The termination resistor value is 120ohms and the size is 1608.
Should I increase the size (2012?) or am I using it incorrectly?
Please provide an answer.
Thank you.