Part Number: TCAN1145-Q1
Tool/software:
Hi Team,
Could you help share the bit width spec for 500Kbps?
D/S only show 2Mbps(above 1 Mbps up to 2 Mbps) and 5Mbps(above 2 Mbps up to 5 Mbps).

BR
Adrian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1145-Q1
Tool/software:
Hi Team,
Could you help share the bit width spec for 500Kbps?
D/S only show 2Mbps(above 1 Mbps up to 2 Mbps) and 5Mbps(above 2 Mbps up to 5 Mbps).

BR
Adrian
Hi Adrian,
Per ISO 11898-2:2016 the limits for those timing parameters are not defined for intended use with bit rates up to 1 Mbit/s. So we don’t have those specifications.
While I don’t have any reference data, I would expect that the deviation at 500khz bit times to match that of the 2Mbps specification in the datasheet, this would result in a tbit(RXD) between 1640ns (-18%) and 2160ns (+8%), tbit(bus) between 1800ns (-10%) and 2100ns (+5%).
Regards,
Sean