Other Parts Discussed in Thread: TCAN4550
Tool/software:
Hello,
I am using the TCAN4550-Q1. I use this IC in test mode and only use GPIO1, GPIO2 to communicate (not using the CANH, CANL) . These GPIOs goes to isolator and than to TCAN1044 (CAN FD BUS TXVR).
My supplies to the TCAN4550 are 3.3V (VIO) and 27V (VSUP). The consumption from the 27V is couple of mAs, and because this circuit is supplied from batteries i want to consume less power as possible.
Can i supply the TCAN4550 only from 3.3V if i don't use the CANH and CANL and only use GPIOs 1,2?
Thank you
Maor M.