Part Number: TCA9539
Tool/software:
Dear TI Team:
I just want to check IO expander_TCA9539RTWR output status.
When one Port of TCA9539RTWR is set to output, it will have 3 status: High,low, and High impedance, Right?
Best Regards
Lisa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9539
Tool/software:
Dear TI Team:
I just want to check IO expander_TCA9539RTWR output status.
When one Port of TCA9539RTWR is set to output, it will have 3 status: High,low, and High impedance, Right?
Best Regards
Lisa
Hi Tyler,Clemens:
Got your points.mostly IC just has two status when set to output, but I saw some will support high impedance(high & low mosfet both off).
And check from the block diagram of TCA9539RTWR, I assume it will also have status with both Q1 & Q2 off when set to output.

BR
Lisa
Hi Lisa,
When the I/O pin is configured to be an OUTPUT, either Q1 or Q2 will be turned ON depending on the values in the output port register (0x02 & 0x03).
If you desire the I/O pin to have Q1 and Q2 disable, configure the I/O pin to be a high-z input through the configuration registers (0x06 & 0x07).
Regards,
Tyler